Error in AN12395 for OM-SE050ARD deep power-down mode for J14

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in AN12395 for OM-SE050ARD deep power-down mode for J14

852 Views
jaredl
Contributor I

Page 8 of AN12395 indicates that J14 must be set to postion 1-2 to enable deep power-down mode.  I believe this is incorrect.  According to the description given, Figure 6, and the settings shown in Table 4, I think it should read:

  • J14: Must be set to position 3-4.

I don't have one of these boards to validate this.  I am just reading through documentation getting ready to build a prototype with the SE050.

0 Kudos
Reply
1 Reply

826 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @jaredl ,

 

Actually in earlier version it is 3-4 for J14  indeed, but I am not sure if it is due to hardware version difference, let me check it with the expert .

 

Thanks for the report!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply