Unable to build using A71CH Configure tool as mentioned in the 7.2 section of the AN12135 document https://www.nxp.com/docs/en/application-note/AN12135.pdf getting the following errors in visual studio.
Did you meet you in the following step?
Would you specify the visual studio version as well as the host sw package? I will try to test it here.
Thanks for your patience!
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Yes, in that step only. It's Visual Studio community 2017 version 15.9.7. How to know the host SW package?
The host sw package is downloaded like below:
The info in red is the Sw version .
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello,
I built both of them, with some error showed "Windows SDK 8.1" needed, and after installation, they are built successfully.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks for the information! Which A71CHConfig project did you open? Would you please clarify?
Thanks for your patience!
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------