The list of registers for SM4.RGSTCHCK, SM4.AIPS_SWCHECK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The list of registers for SM4.RGSTCHCK, SM4.AIPS_SWCHECK

289 Views
HeebeomPark
Contributor II

Can you specify the list of the registers between SM4.RGSTCHCK and SM4.AIPS_SWCHECK? 

HeebeomPark_0-1711553452624.pngHeebeomPark_1-1711553468267.png

We opened S32K3xx_REG_PROT_detail.xlsx however it looks it is somehow duplicated with the following registers, which was informed by NXP.

RegisterCategory
Crossbar Integrity Checker (HSE_B & AES_ACCEL AXBS_Lite) ERM_1SR
Software Watchdog 3 Trigger Multiplexing Control Body Cross Triggering UnitSR
eMIOS_0
eMIOS_1
eMIOS_2 
SR-AD
Logic Control Unit 0 Logic Control Unit 1 SR-AD
System crossbar switch Crossbar Integrity Checker (System AXBS / AXBS Lite)
Crossbar Integrity Checker (Peripheral AXBS-Lite)
SR
eDMA control & status (MP_CSR; MP_ES; MP_HRS)
eDMA transfer control descriptor 0
eDMA transfer control descriptor 1
eDMA transfer control descriptor 2
eDMA transfer control descriptor 3
eDMA transfer control descriptor 4
eDMA transfer control descriptor 5
eDMA transfer control descriptor 6
eDMA transfer control descriptor 7
eDMA transfer control descriptor 8
eDMA transfer control descriptor 9
eDMA transfer control descriptor 10
eDMA transfer control descriptor 11 
SR
RAM controller 0SR
Flash controller
Flash controller alternate
SR
Software Watchdog 0SR
System Timer Module 0 XRDCSR
Interrupt Monitor DMA Channel Multiplexer 0 DMA Channel Multiplexer 1 Real-time clock Reset Generation ModuleSR
32 kHz Slow Internal RC OscillatorSR
32 kHz Slow External Crystal OscillatorSR
48 MHz Fast Internal RC OscillatorSR
8-40 MHz Fast External Crystal Oscillator Clock Generation Module Mode Entry ModuleSR
Frequency Modulated Phase-Locked Loop
Frequency Modulated Phase-Locked Loop 2
SR
Power management controllerSR
Flash memory
Flash memory alternate
SR
Programmable Interrupt Timer 2
Programmable Interrupt Timer 3
SR
FCCU (+FOSU) MU_0_MUB
JDC (JTAG Data Communication) Configuration GPR
SR
Self-Test Control UnitSR
0 Kudos
1 Reply

283 Views
john_floros
NXP Employee
NXP Employee

Hello,

It is really the same registers.  The AIPS allow you to gain access to the peripheral registers with the use of three AIPS busses for the S32K388.  See diagram below.  Essentially for the AIPS check you would just need to check the value of registers that would excercise all three AIPS busses to verify the AIPS.  For the Safety register check you would need to select safety relevant, for your application, registers and verify that the values what you would expect.

john_floros_0-1711575756302.png

Regards,

John

 

0 Kudos