SM2 and SM1 Scheduling sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SM2 and SM1 Scheduling sequence

跳至解决方案
243 次查看
FabioG
Contributor III

Hi There,

In developement of Safety Mechanisms, which is the right  scheduling sequence ? I suppose that SM2 run  before SM1. Is it correct? Or is  it true  the opposite way? Or there is no a fixed order ?

For example:  "SM2.CMU.sCheck" should be run before "SM1.CMU_FC" and "SM1.CMU_FM", because first  is necessary to check if fhe hardware is ok, then it is possible to use CMU for check frequency and measure period. Is it righi ? If yes, is it for all SM1 and 2?

Best Regards,

Fabio

0 项奖励
1 解答
212 次查看
antoinedubois
NXP Employee
NXP Employee

Hi Fabio,

SM1 define HW Safety Mechanisms, SM2 define SW Safety Mechanisms, it is different than Safety Mechanisms for SPF vs LF.

But in general, it is often he case that the latent fault safety mechanisms is implemented in SW so it is often and SM2.

Then you can probably see in the reference Manual that Safety Mechanisms used for latent fault should be perform within your MPFDTI of your systems. Depending of you timing you can have different strategy:

- Run all your latent fault safety mechanisms at Vehicle Key-ON, MCU Start-up. It is the simplest in term of SW development, but it may increase your start-up time. Your example for clock is the perfect example for that

- Run all of them at Key-OFF, or during Run time (but not during your Safety related operational Mode).

- Use some cyclic combination to make sure it is run once per MPFDTI.

 

I hope it helps

Antoine

 

 

在原帖中查看解决方案

0 项奖励
1 回复
213 次查看
antoinedubois
NXP Employee
NXP Employee

Hi Fabio,

SM1 define HW Safety Mechanisms, SM2 define SW Safety Mechanisms, it is different than Safety Mechanisms for SPF vs LF.

But in general, it is often he case that the latent fault safety mechanisms is implemented in SW so it is often and SM2.

Then you can probably see in the reference Manual that Safety Mechanisms used for latent fault should be perform within your MPFDTI of your systems. Depending of you timing you can have different strategy:

- Run all your latent fault safety mechanisms at Vehicle Key-ON, MCU Start-up. It is the simplest in term of SW development, but it may increase your start-up time. Your example for clock is the perfect example for that

- Run all of them at Key-OFF, or during Run time (but not during your Safety related operational Mode).

- Use some cyclic combination to make sure it is run once per MPFDTI.

 

I hope it helps

Antoine

 

 

0 项奖励