S32k11x for ASIL-A: Internal watchdog only?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k11x for ASIL-A: Internal watchdog only?

Jump to solution
407 Views
AdrianR
NXP Employee
NXP Employee

Safety measure SM_041 specifies the need of external monitoring (e.g. watchdog or comm) to be able to reach ASIL-B levels.

What about for a ASIL-A level design - is external monitoring still mandatory for S32K11x?

Labels (1)
Tags (1)
0 Kudos
1 Solution
361 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this discussion as solved, due to a migration of a new community platform.
If you have additional questions, please create a new post and reference to this closed thread.

NXP Community!

View solution in original post

0 Kudos
2 Replies
362 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this discussion as solved, due to a migration of a new community platform.
If you have additional questions, please create a new post and reference to this closed thread.

NXP Community!
0 Kudos
370 Views
aarul
NXP Employee
NXP Employee

Hi Adrian

As discussed over email, external monitoring is required but you don't need to have a specific hardware implementation for it. The text below the assumption describes that "periodic external communication involving the execution core on MCU can serve the purpose of external monitoring". The assumption is important to ensure the case where MCU is no longer responding and is unable to go into safe state. This monitoring ensures that system will still go into safe state.

Regards

-Aarul

0 Kudos