S32K148 Safety Manual SM_116 + SM_117

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 Safety Manual SM_116 + SM_117

390 Views
hochs2
Contributor II

Hello,

We have a requirement to satisfy SM_116 and SM_117. Our system is already performing memory checks (ECC) for the Flash memory. Would these checks cover the requirements for SM_116 and SM_117?

Thank you,

Hunter

Labels (1)
0 Kudos
1 Reply

348 Views
nxf61080
NXP Employee
NXP Employee

Hi Hunter,

Please find the relevant explanation regarding both the assumptions:

1) SM_116:  This assumption requires one to check for:

                    Multibit errors introduced by permanent failure in flash controller

                    Perform flash integrity checks

                    Save safety-relevant code/data with CRC or hash signature to detect any Integrity violation

To address these issues we need to have the following safety mechanisms:

The Flash array integrity check as a safety mechanism. The array integrity self-check is used to detect possible latent faults affecting the flash array and can be initiated by the software. The flash array integrity check computes a MISR signature which the application software can then compare with a previously known value.

A safety mechanism for ensuring the pass status of previous flash operations. This safety mechanism gives information about the outcome of any program/erase operation. This mechanism is enabled by default and the relevant register bit must be checked by software after a program/erase operation.

 For storing safety-relevant code/data the assumption advises using CRC/hash signatures.

2)SM_117: This assumption requires the use of a software safety mechanism to ensure the correctness of any write operation performed on flash. This assumption can be satisfied by using CRC checks.

 For performing all CRC related checks the built-in hardware CRC module can be used.

To sum up, ECC checks aren’t sufficient to satisfy all the required conditions for SM_116 and SM_117 and some additional measures are required as stated above.

Hope this helps!

Thanks and regards,
Manibha

0 Kudos