[Medini files]S32K3xx customized FMEDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Medini files]S32K3xx customized FMEDA

Jump to solution
319 Views
binli
NXP Employee
NXP Employee

Hi:

Just want to confirm that whether we could release K3xx fmeda Medini file to customer?

  • If yes, does MediniAnalyze version must be 2021 R2?
  • If yes, could be via secure file or other ways?

My customer baught Ansys Mediti tool already, they want to make FMEDA with their own configuration.

Thanks a lot.

 

Labels (1)
Tags (1)
0 Kudos
1 Solution
291 Views
Yashwant_Singh
NXP Employee
NXP Employee

Hello,

Yes the medini files for the S32K3xx family are available upon requests. Ansys release different version each year so the .mprx files for different products in the family are available under different versions however Medini allows migrating files to newer versions of the tool and so we would recommend using the latest one (2023 r2 or newer).

Secure files is the official channel for release however it can also be done via a common sharepoint link or drive with the customer.

Thanks!

-Yashwant

 

 

View solution in original post

0 Kudos
2 Replies
292 Views
Yashwant_Singh
NXP Employee
NXP Employee

Hello,

Yes the medini files for the S32K3xx family are available upon requests. Ansys release different version each year so the .mprx files for different products in the family are available under different versions however Medini allows migrating files to newer versions of the tool and so we would recommend using the latest one (2023 r2 or newer).

Secure files is the official channel for release however it can also be done via a common sharepoint link or drive with the customer.

Thanks!

-Yashwant

 

 

0 Kudos
271 Views
binli
NXP Employee
NXP Employee

Hi Yashwant:

Got it, thanks a lot.

0 Kudos