EIM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EIM

237 次查看
HeebeomPark
Contributor II

In the FMEDA, there is no safety mechanism for EIM1/2/3 and the comment is written like "EIM cannot be activated with a single bit.". In this case, what is the recommendation for safety application?

Can you explain in more detail? 

HeebeomPark_0-1717631835087.png

 

0 项奖励
1 回复

110 次查看
antoinedubois
NXP Employee
NXP Employee

Hello,

EIM are the feature to test the safety mechanisms therefore if they fail they would be consider triple point fualt and are consider safe.

The only potential failure mode is the unintended activation of the EIM, however in the HW there is a dual enable and Triple voting flogs therefore it cannot happen. There is no specific implementation required by the customer it is built into the HW.

0 项奖励