Are the VDD_HV_A/VDD_HV_B/V15/VSS pins connected inside the device on S32K3 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are the VDD_HV_A/VDD_HV_B/V15/VSS pins connected inside the device on S32K3 ?

485 Views
hirokado
Contributor III

Hello Support team,

I have a question about S32K314 from the viewpoint of functional safety.

[Questions]
"VDD_HV_A / VDD_HV_B / V15 / VSS" have multiple pins, and these pins should be connected on their board.
Are they also connected inside the device?

[Background]
My customer is asking from a functional safety perspective.
Therefore, they are concerned about whether it can still operate even if one pin fails.
I understand that the performance will drop, but I want to check if it works as a function.

Best regards,
Hiroyuki Kadowaki

Labels (1)
0 Kudos
2 Replies

471 Views
Yashwant_Singh
NXP Employee
NXP Employee

Hi Hiroyuki,

The multiple supply pins for a single supply are connected inside however we have not analyzed the behavior of the device when one supply pin fails - the device may or may not become reliable. In either case we expect the internal voltage monitoring or the external watchdog to detect a fault and indicate safe state to the external system.

Hope this helps !

Thanks!

-Yashwant

0 Kudos

466 Views
hirokado
Contributor III

Dear Yashwant,

Thank you for your reply.

It's very helpful for me.

I understand your answer.

Best regards,

Hiroyuki Kadowaki

0 Kudos