S23V234 platform:the max current per power supply

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S23V234 platform:the max current per power supply

5,171件の閲覧回数
YMS_Yuanming_Shu
NXP Employee
NXP Employee

1.do you have the detail list that the max current per power supply about the s23v234 platfrom?because many customers request the detail table for deigning the product's power domain.

   the name of per power supply table is as below:

   VDD_DDR_IO/VDD_HV_DDR(1/2/3)/VDDIO_LFAST/VDD_HV_IO_ETH(1/2)/VDD_HV_IO_FLA/VDD_HV_IO_DIS(1/2/3)/VDD_HV_IO_VIU0(1/2)/VDD_HV_IO_VIU1/VDD_GPIO0/VDD_GPIO1/VDD_GPIO2/VDD_LV_POST

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

4,725件の閲覧回数
tombrown
NXP Employee
NXP Employee

Hello Sym,

This forum is no longer active.

I will work with you offline on these questions.

Regards,

Tom

0 件の賞賛
返信

4,725件の閲覧回数
YMS_Yuanming_Shu
NXP Employee
NXP Employee

okay,thanks!

0 件の賞賛
返信