Hi,
I have modified I2C pins according to our custom board.
While kernel booting it getting failed message but it is successfully configured.
[ 0.891190] s32v234-siul2 4006c000.siul: failed to get pin(15) name
I think we need to change the PAD name. I could not understand where we need to change in kernel source code.
Can you please help on this.
Thanks in advance.
Thanks,
Ramanjineyulu.
Hi Ramanjineyulu,
It sounds like a BSP configuration issue, maybe you have to ask for help from your account manager or local FAE on the support for s32v234 custom board, and I will move this thread to the Auto community, you may get more help from there.
Best regards,
Kan
for me it sounds like you have altered the device description file that is loaded (in a pre-compiled variant) along with the linux kernel at early boot stage by u-boot.
you might want to show here what changes you have applied to this file.