Hi asd046012,
All pins keep the default state, this is, Analog pins remain the analog function, digital pins are disabled, in other words in high impedance(tri-stated).
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi asd046012,
All pins keep the default state, this is, Analog pins remain the analog function, digital pins are disabled, in other words in high impedance(tri-stated).
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Robin,
I know that I am a bit late in the topic but I want a clarification if possibile:
When the MCU is KEPT in RESET, what is the status of the ports?
I'm asking because the datasheet specifies the status out of reset or port not initialized.
Also, if the MCU is NOT powered (e.g. FS applications that cut off MC power) what is the status of the mcu ports?
Thanks and K.R.