what is the file format of EPC/EPD? in mcal , autosar

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the file format of EPC/EPD? in mcal , autosar

ソリューションへジャンプ
715件の閲覧回数
focusdoit
Contributor III

what is the abbrevation of .epd .epc in Mcal? 

Thanks

0 件の賞賛
返信
1 解決策
688件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @focusdoit

EPD/EPC files are BSW Module Description/Configuration files (or AUTOSAR module definition file) which can also be used in XDM format.

EPD is the standard AUTOSAR format. This allows the AUTOSAR software to be used with any other AUTOSAR Configuration/Generation tool.

XDM is a proprietary format (EB) providing enhanced usability features during configuration with EB tresos Studio.

Julin_AragnM_0-1710958020141.png

Best regards,
Julián

 

元の投稿で解決策を見る

1 返信
689件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @focusdoit

EPD/EPC files are BSW Module Description/Configuration files (or AUTOSAR module definition file) which can also be used in XDM format.

EPD is the standard AUTOSAR format. This allows the AUTOSAR software to be used with any other AUTOSAR Configuration/Generation tool.

XDM is a proprietary format (EB) providing enhanced usability features during configuration with EB tresos Studio.

Julin_AragnM_0-1710958020141.png

Best regards,
Julián