Hi,
I would like to implement VLPS mode, then wakeup by timer on s32K144. I can set s32k144 to VLPS mode, and wakeup by interrupt-GPIO. But no idea about how to wakeup by timer. Could you share some experiences with me for my purpose?
解決済! 解決策の投稿を見る。
It does not.
Enable it by the Clock and LPIT drivers.
For example, in the PE GUI of DS2.2 IDE
BR, Daniel
Hi Daniel,
I use the following API to VLPS. Does the API include "SCG_SIRCCSR[SIRCSTEN = 1, SIRCLPEN = 1" and "LPIT_MCR[DOZE_EN] = 1"?
POWER_SYS_SetMode(VLPS, POWER_MANAGER_POLICY_AGREEMENT);
It does not.
Enable it by the Clock and LPIT drivers.
For example, in the PE GUI of DS2.2 IDE
BR, Daniel
Hi @jacqueshsu,
As you can see in the RM, Table 7-8. AWIC stop and VLPS wake-up sources, you can use the LPIT timer.
LPIT is functional in VLPS if the function clock of this module is SIRC and LPIT_MCR[DOZE_EN] = 1.
The SIRC clock must be enabled in VLPS (SCG_SIRCCSR[SIRCSTEN = 1, SIRCLPEN = 1).
BR, Daniel
Hi Daniel,
I need this function, too. could you please help me?