tickless freertos LPTM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tickless freertos LPTM

903 Views
david_lion1
Contributor I

Hi, 

I try to use FreeRTOS on S32K144, but I am blocked on a timing problem.

I use the tickless feature with LPTM.

For periodic task without any external interrupt I have no problems.

But, when I have external interrupt I have a problem. The calculation  when something other than the tick interrupt ended the sleep seems to be ok for me. But I have sometimes extra time, so my periodic task drift ...

Do you have any ideas for my problem ? 

Here the source code used :

/* Determine if LPTM interrupt occured */
if(isTimerInterruptFire == TRUE )
{
isTimerInterruptFire = FALSE;
uint32_t ulCalculatedLoadValue;

/* The tick interrupt is already pending, and the LPTM count
reloaded with ulReloadValue. Reset the
CMR register with whatever remains of this tick
period. */
ulCalculatedLoadValue = ulTimerCountsForOneTick - luw_time_ref;

/* Don't allow a tiny value, or values that have somehow
underflowed because the post sleep hook did something
that took too long. */
if( ( ulCalculatedLoadValue < ulStoppedTimerCompensation ) || ( ulCalculatedLoadValue > ulTimerCountsForOneTick ) )
{
ulCalculatedLoadValue = ( ulTimerCountsForOneTick );
}

LPTMR0->CMR = ulCalculatedLoadValue;

/* As the pending tick will be processed as soon as this
function exits, the tick value maintained by the tick is stepped
forward by one less than the time spent waiting. */
ulCompleteTickPeriods = xExpectedIdleTime - 1UL;
}
else
{
/* Something other than the tick interrupt ended the sleep.
How many complete tick periods passed while the processor
was waiting? */
ulCompleteTickPeriods = luw_time_ref / ulTimerCountsForOneTick;


/* The reload value is set to whatever fraction of a single tick
period remains. */
ulCompletedSysTickDecrements = ulTimerCountsForOneTick - (luw_time_ref - ulCompleteTickPeriods*ulTimerCountsForOneTick);
/* The reload value is set to whatever fraction of a single tick
period remains. */
LPTMR0->CMR = ulCompletedSysTickDecrements;

}

/* Restart LPTM so it runs from CMR register
again, then set CMR register back to its standard
value. */
LPTMR0->CSR |= LPTMR_CSR_TEN(1); // timer enable
vTaskStepTick( ulCompleteTickPeriods );

Thanks a lot ! 

David

Labels (1)
0 Kudos
Reply
0 Replies