the PLL error of the s32k312 in ppm

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the PLL error of the s32k312 in ppm

699 次查看
dongyong1
Contributor I

Dear NXP Engineers

 

I would like to know what is the PLL error of the s32k312 in ppm

0 项奖励
4 回复数

670 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @dongyong1 

Sorry for the inconvenience this may cause. 

All information related to the PLL jitter is provided in Table 41 of the S32K3xx Data Sheet, Rev. 8.

 

B.R.

VaneB

0 项奖励

655 次查看
dongyong1
Contributor I

Hi VaneB

take the last line of Table41 as an example(1680ps 120Mhz). Is it possible to calculate like this: 1/120MHZ=8.3ns, 1680ps/8.3ns=0.2. (0.2/120M)*1000000=0.002ppm

dongyong1_0-1692841739259.png

 

0 项奖励

589 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @dongyong1 

These two specs are about entirely different things. So, I think converting the ps to ppm is not possible. 

Frequency is the number of cycles executed per second. Otherwise, the jitter is about the variance of the clock period. So, if your clock period varies randomly by 10ns RMS (for example), but the period is still 1µs on average, then you can have a very accurate (but jittery) 1MHz clock.

0 项奖励

632 次查看
dongyong1
Contributor I
Hi @VaneB

Is that right?
0 项奖励