Hi NXP Team,
For my project i am using S32K342 with EBTresos for configuration and Autosar OS. I am facing sram memory block doesn't fit mcal_bss segment issue as below.
Linking main.elf
[elxr] (error #310) section .mcal_bss (0x204082e0-0x20408837) doesn't fit in memory block int_sram (0x20400000-0x204087ff)
make: *** [makefile:266: main.elf] Error 1
I have already extended the sram region from default 28KB to 34KB after checking the datasheet. If i extend another 1KB which is to 35KB i got Software breakpoint issue at IntCtrl_Ip.c line number 189
DevAssert(S32_SCB->VTOR >= (uint32)__INT_SRAM_START);
Can i place the entire sram section in DTCM which is part of SRAM and the allocated memory size also bigger (128KB).
I have attached my project memory segment screenshot and the default memory segment screenshot from RTD SPI_example. Please help me to fix the issue.