s32k3 HSE BSB IVT question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k3 HSE BSB IVT question

Jump to solution
429 Views
victory
Contributor III

Hi NXP,

for S32K3 basic secure boot,  it related to IVT configuration, here is 2 question:

1. IVT has cm7_0_reset_address and APPBL address,  if both address are valid,  mcu how to determine which one to run?

2. IVT header and app_bl both have AuthTag,  is IVT_AUTH is set, is both GMAC tag required  or optional?

thanks.

0 Kudos
Reply
1 Solution
392 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) AppBL is an authenticated application image, that can run in the host instead of the Apps.
The "Apps" are the first executable to run in the host during normal operation after reset. Alternatively, "AppBL" can run in the host after HSE verification.
And Basic Secure Boot supports booting one target core (AppBL).

2) Seem to be required.

3) If you are in basic secure mode and you have configured one target core, you should boot with "AppBL" address.

View solution in original post

0 Kudos
Reply
4 Replies
393 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) AppBL is an authenticated application image, that can run in the host instead of the Apps.
The "Apps" are the first executable to run in the host during normal operation after reset. Alternatively, "AppBL" can run in the host after HSE verification.
And Basic Secure Boot supports booting one target core (AppBL).

2) Seem to be required.

3) If you are in basic secure mode and you have configured one target core, you should boot with "AppBL" address.

0 Kudos
Reply
412 Views
victory
Contributor III
i set ivt appbl (0ffset 0x30) and have valid appbl header and app code, after reset, mcu run the boot code(0x400000), not jump to 0x501fc0 (appbl) code.
0 Kudos
Reply
370 Views
victory
Contributor III
appbl address valid, and ivt header set BOOTSEQ, it run appbl instead of CM7_0 address.
0 Kudos
Reply
359 Views
victory
Contributor III
appbl address valid + appbl  taged + ivt header set BOOTSEQ,   it run appbl instead of CM7_0 address.
0 Kudos
Reply