s32k116 The power light does not light up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k116 The power light does not light up

跳至解决方案
2,518 次查看
liuxing_hu
Contributor III

Just received the development board soon, when I powers the S32K116-EVB from USB power supply, the corresponding light does not light up, even push reset button, no light light up.

0 项奖励
回复
1 解答
2,496 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

D3 not light. Seems not powered. Have you try to use another USB cable or another USB port of PC?

check voltage.jpg

 

Please measure the voltage:
VDD at J10 Pin2
P5V0 at J10 pin3

MCU Power Supply - Jumper Selection.png

 

P5V0 at J107 pin2
P5V_SDA_PSW at J107 pin3J107 P5V_SDA_PSW.png

 

P5V_SDA 

P5V_SDA.png

在原帖中查看解决方案

7 回复数
2,515 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi liuxing_hu,

Please follow the Getting Started with S32K116 Evaluation Board. Our engineer mentioned in the video: Please make sure the J107 is connect 2-3, this makes board powered by USB port.

Getting Started with S32K116 Evaluation Board.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,503 次查看
liuxing_hu
Contributor III

Can you help me confirm whether the connector is ok by attachment, my colleague help me check the connect is ok, but the light doesn't work

0 项奖励
回复
2,497 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

D3 not light. Seems not powered. Have you try to use another USB cable or another USB port of PC?

check voltage.jpg

 

Please measure the voltage:
VDD at J10 Pin2
P5V0 at J10 pin3

MCU Power Supply - Jumper Selection.png

 

P5V0 at J107 pin2
P5V_SDA_PSW at J107 pin3J107 P5V_SDA_PSW.png

 

P5V_SDA 

P5V_SDA.png

2,442 次查看
liuxing_hu
Contributor III

my colleague help me to find that USB cable is the reason, before that I have tried 2 USB cables, it didn't work, could you give me the link to bug USB cable? I'm afraid I bought a fake cable

0 项奖励
回复
2,493 次查看
liuxing_hu
Contributor III

thanks very much for your detailed information, I will try

0 项奖励
回复
2,513 次查看
liuxing_hu
Contributor III

do you means that I need to connect pin2 and pin3 of J107 ?

0 项奖励
回复
2,508 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

yes

S32K116EVB-QSG.png