Hi,
I work with the S32k144 and design studio 2018.R1.
I tried to import and debug a project, but:
these errors appear after importing the project and:
these join them after I build 'Debug_Flash'.
In another post installing 'gcc-arm-none-eabi-10-2020-q4-major-win32.exe' was the solution, but I just installed it and there is no change.
Hope someone knows what this means.
Best regards,
Raphael
Solved! Go to Solution.
Installing S32 Design Studio 3.4 and adding Service pack 1 solved my problem
One solution would be to set the PATH variable to a toolchain of choice, either per project or to the entire editor, as shown below:
Installing S32 Design Studio 3.4 and adding Service pack 1 solved my problem