openSDA USB connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

openSDA USB connection

571 Views
ankan_creatara
Contributor III

Hello everyone,

I am back with some other doubts. Kindly take out some time to help me out.

I am attaching the screenshot of the opensda schematic input via USB. I have the following doubts:
1. What are these L1 and L2? I believe these are inductors. If yes, then why is its value in OHMS?
2. Why are these L1 and L2 used and connected? I understand the use of bypass capacitors along with the power source; but I couldnot figure out the use of these L1 and L2.
3. Also, kindly help me out in figuring the use of D17, D18 and D19 in the circuit.

ankan_creatara_0-1665569076916.png
Kindly help me out in understanding the schematic.

Thank you for your time.

 

0 Kudos
Reply
1 Reply

566 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) L1 and L2 are ferrite beads and 330Ohm is an impedance at 100MHz. If you want to see specific type, for instance following:
MPZ1608S331A

2) https://en.wikipedia.org/wiki/Ferrite_bead

3) It is ESD protection diode.

https://www.nexperia.com/products/esd-protection-tvs-filtering-and-signal-conditioning/esd-protectio...

0 Kudos
Reply