not download s32k116

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

not download s32k116

877 次查看
jinsheng20
Contributor III

hi:

   Before the board is easy to use, through JFLASH erase the entire slide after this, the connection is OK。

  • What do I need to do

 

SEGGER J-Link GDB Server V6.42a Command Line Version

JLinkARM.dll V6.42a (DLL compiled Feb 1 2019 18:00:08)

Command line: -if swd -device S32K116 -endian little -speed 1000 -port 2331 -swoport 2332 -telnetport 2333 -vd -ir -localhostonly 1 -singlerun -strict -timeout 0 -nogui
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: on
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: S32K116
Target interface: SWD
Target interface speed: 1000kHz
Target endian: little

Connecting to J-Link...
J-Link is connected.
Firmware: J-Link V10 compiled Jun 9 2020 13:38:07
Hardware: V10.10
S/N: 260106173
Feature(s): FlashBP, GDB, FlashDL, JFlash, RDI
Checking target voltage...
Target voltage: 4.64 V
Listening on TCP/IP port 2331
Connecting to target...ERROR: Could not find core in Coresight setup
ERROR: Could not connect to target.
Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...
Shutting down...
Could not connect to target.
Please check power, connection and settings.

0 项奖励
回复
2 回复数

868 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

It looks like you have secure the device somehow.

What did you do with the device? Could you provide more details?

best regards,

Peter

0 项奖励
回复

860 次查看
jinsheng20
Contributor III

I used JFlash to connect jLink to JLINK in SWD mode and erased the whole thing. I've done this before to erase analog EEPROM data without a problem, but this time it's done

0 项奖励
回复