making multiple adc hardware unit in S32DS GUI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

making multiple adc hardware unit in S32DS GUI

584 Views
gkunalupta
Contributor III

Hi their,

I am using and in that using ADC instance 0 using NXP S32K144 Microcontroller. But of ADC instance i want to configure ADC0CH12 and ADC0CH1 with different properties in GUI.

But in GUI if i create new hardware unit but with same ADC instance number, then it shows S32Ds shows error.

 

Why is it so?? Cant i create multiple ADC hardware unit of same ADC instance but withy different features??? 

If not so is kind of limitation, but then it becomes compulsary for me to use ADC0 all channels with same configuration.

What i am having planning to have is, to have multiple hardware units of same ADC instance, so that i can configure different channels of same ADC isnatnce with differnet features. Cant i do that.

gkunalupta_0-1722202908346.png

 

Tags (3)
0 Kudos
Reply
6 Replies

495 Views
Kunal_Gettobyte
Contributor III

Any reply???

0 Kudos
Reply

481 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you share your project?

0 Kudos
Reply

407 Views
gkunalupta
Contributor III

Any replies?

0 Kudos
Reply

469 Views
gkunalupta
Contributor III
 
0 Kudos
Reply

554 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Which example is this related to? Also please specify used RTD/SDK. Thanks

0 Kudos
Reply

531 Views
gkunalupta
Contributor III

This is the SDK.

And no example, am creating a project from scratch.

Using ADC module Driver of Autosar RTD 1.0.0

gkunalupta_0-1722326148918.png

 

0 Kudos
Reply