I installed two vesion MCAL.
My peoject base on old version.
I want upgrade module configurations to new module versions.
But there is no new version in upgrade window.
The installation steps are as follows:
Hello,
You're right. Unfortunately, due to that derivate change, you need to create a new project based no RTM 1.0.5, then import the configuration from RTM 1.0.0 to that new project.
Best Regards,
Nam
I found that the derivate of the two versions do not match.This is why it can't be updated.