ftm pwm clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ftm pwm clock

1,995件の閲覧回数
2684743015
Contributor I

Hi, NXP  teams,

I have some problems in S32K 146 ftm pwm mode,

when I used FTM mode,I used FTM3 mode ,but all the FTM clock source are opend ,then I turn off the extra clock source of FTM and use PE to generate code and save it .    And the second time when I opened the project ,all the FTM clock has been opened again, I don't know why .  Could you help me ?

Kindly help me, Thanks in advance.

 

Regards,

Liu chao

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

1,797件の閲覧回数
2684743015
Contributor I

Hi,  Daniel,

   I use s32k146_SDK   2.0.0

pastedImage_1.png

All of my  projects behave like this in s32k146.

0 件の賞賛
返信

1,797件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Liu,

Thank you, I can reproduce the issue with SDK RTM 2.0.0.

But it works with SDK RTM 3.0.0.

I will try to find more information about it.

BR, Daniel

0 件の賞賛
返信

1,797件の閲覧回数
2684743015
Contributor I

Hi, Daniel,

   Thank you for your help,  my  colleague  has same problem with  SDK RTM 3.0.0.

BR, LiuChao

0 件の賞賛
返信

1,797件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello LiuChao, 

Sorry for the confusion, the issue has been already fixed but with the SDK v3.0.1 release.

BR, Daniel

0 件の賞賛
返信

1,799件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

HI Liu,

I can't reproduce this with the up-to-date S32DS.

What version of the S32DS are you using?

Is this an issue of a single project or all you projects behave like this?

Thanks,

Daniel

0 件の賞賛
返信