fs2322b

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
321 Views
zq1
Contributor III

i am building a project with a sbc called fs2322b ,but there is no examples can be helpful ,what i can find is only below ,but it is not useful for me,

企业微信截图_17027186697391.png

 so is there some other example that can be provided to me ,thank you .

then, when i read the datasheet of fs2322,there are some verbs i can not understand ,like below:

zq1_0-1702718981973.png

what's meaning of otp fuse,i need your help ,as soon as possible,

0 Kudos
1 Solution
286 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

I am not aware of any other FS23 software drivers and code examples.

OTP fuse means that the value of these bits depends on their OTP configuration. For example, the LIN_EN bit will be 0 (= LIN disabled) if the corresponding LIN_EN_OTP bit is 0. Similarly, the LIN_EN bit will be 1 (= LIN enabled) if the LIN_EN_OTP bit is 1.

In case of the FS2322B, LIN_EN_OTP = 0 (= LIN disabled) and consequently LIN_EN is also 0.

Capture.JPG

BR, Tomas

View solution in original post

0 Kudos
1 Reply
287 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

I am not aware of any other FS23 software drivers and code examples.

OTP fuse means that the value of these bits depends on their OTP configuration. For example, the LIN_EN bit will be 0 (= LIN disabled) if the corresponding LIN_EN_OTP bit is 0. Similarly, the LIN_EN bit will be 1 (= LIN enabled) if the LIN_EN_OTP bit is 1.

In case of the FS2322B, LIN_EN_OTP = 0 (= LIN disabled) and consequently LIN_EN is also 0.

Capture.JPG

BR, Tomas

0 Kudos