external Debugger / programmer JTAG tool for S32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

external Debugger / programmer JTAG tool for S32k144

3,109 Views
pietroserao
Contributor II

Good morning,

i'm in hardware design phase, i need to know which device allow me to debug / program my board.
I need to use a 10 pin jtag connector.

There is something ready to use?

 

I'm using a S32k144 microcontroller.

 

Thank you.

Labels (1)
0 Kudos
Reply
1 Reply

2,242 Views
martin_kovar
NXP Employee
NXP Employee

Hi Pietro,

please look at the following link. In section Emulators/Probes are listed all devices, which could be used for debugging/programing S32k144.

32-bit Automotive General Purpose MCUs|NXP 

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 Kudos
Reply