compilation Fail SDK_32XX_4.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

compilation Fail SDK_32XX_4.0.0

Jump to solution
596 Views
monk_65
Contributor III

 

Hi,

when I create a new project with S32K344, compilation work

but if i configure a pin and update code,compilation failed

directory platform install is \NXP\S32\S32DS\software\PlatformSDK_S32XX_4_0_0\RTD\Base_TS_T40D11M40I0R0

 

but message is

D:/NXP/S32/S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M40I0R0/include/OsIf_Internal.h:45:10: fatal error: OsIf_Cfg.h: No such file or directory

when I compile

 

0 Kudos
Reply
1 Solution
424 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@monk_65

Have you installed multiple RTD versions under one S32 DS?

Installing different RTD versions under the same S32 DS will cause some similar errors.

This is somewhat similar to what I told you before.

If possible, you can uninstall the IDE and reinstall it and Please remember to delete all files in the installation directory.

View solution in original post

0 Kudos
Reply
11 Replies
315 Views
monk_65
Contributor III

i reinstall package and my problem has resolved

 

 

0 Kudos
Reply
560 Views
monk_65
Contributor III

Capture.PNGCapture1.PNG

 

thanks,

to have more information, here the message when i select peripheral

my configuration is S32K344, why is not compatible ?

 

0 Kudos
Reply
526 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@monk_65

Does this project come from S32DS?

Have you installed multiple RTD versions under one S32 DS?

Installing different RTD versions under the same S32 DS will cause some similar errors.

Please be sure to install a separate S32 DS for each RTD versions.

0 Kudos
Reply
558 Views
spara7c5
Contributor III

Have you properly started from demo project for S32K344? please check

0 Kudos
Reply
571 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@monk_65

Please try opening a sample project from S32 DS and test if such problem still exists.

If yes, it may be an issue with the RTD installation

If not, check your project and compare the difference between the two projects.

0 Kudos
Reply
574 Views
spara7c5
Contributor III

It seems you have not generated the OS code. Please check in the Peripheral setup, in OS>Generate you find Generate Configuration button. Press it and then update the code

0 Kudos
Reply
481 Views
monk_65
Contributor III

i reinstalled package with S32 extensions and updates

RTD S32K3_S32M27X 4.0.0.202404020208 com.nxp.RTD.S32K3_S32M27X.root.feature.feature.group NXP Semiconductors, Inc.

RTD S32K3XX 4.0.0.202404020208 com.nxp.RTD.S32K3XX.root.feature.feature.group NXP Semiconductors, Inc.

S32K3xx development package 3.5.8.202311290134 com.nxp.s32ds.s32k3.dev.feature.feature.group NXP

S32 Design Studio for S32 Platform 3.5.11.202403280939 com.nxp.s32ds.platform.ide.feature.feature.group NXP

FREERTOS S32K3_S32M27X 4.0.0.202312180411 com.nxp.FREERTOS.S32K3_S32M27X.root.4.0.0.feature.feature.group NXP Semiconductors, Inc.

i create a project with a guide_started_s32k_3xx and compilation is OK

but i tried to configure a pin and i have a error

 

 

D:/NXP/S32DS.3.5/S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M40I0R0/include/OsIf_Internal.h:45:10: fatal error: OsIf_Cfg.h: No such file or directory

i don't understand  why  this file is not inside my project

when i use the "manager SDK component"

i selected "OS" package and i have files related in OS in my project

 



 

0 Kudos
Reply
455 Views
spara7c5
Contributor III

Because you have not generated the OS. Press the generate button in peripheral>>OS>>general. And update the project

0 Kudos
Reply
457 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@monk_65

Senlent_0-1715827113600.png

 

 

0 Kudos
Reply
434 Views
monk_65
Contributor III

update_code.PNG

 

but i don't have peripheral , components view, and Osif configuration so i can't add this file

 

when i click on the peripherals tools,  it display  "The peripheral tool is enabled but it does not support the selected processor"

 

0 Kudos
Reply
425 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@monk_65

Have you installed multiple RTD versions under one S32 DS?

Installing different RTD versions under the same S32 DS will cause some similar errors.

This is somewhat similar to what I told you before.

If possible, you can uninstall the IDE and reinstall it and Please remember to delete all files in the installation directory.

0 Kudos
Reply