Hello NXP,
"""
#define FIFO_NUM (3u) /*Fifo num*/
#define TOTAL_FIFO_BYTES (500u + 99u) /*config total bytes*/
#define STRUCT_LEN (20u) /*every fifo struct used space*/
#define TOTAL_BYTES ((STRUCT_LEN) * (FIFO_NUM) + TOTAL_FIFO_BYTES) /*config total bytes*/
"""
This is code from S32K144_UDS_BOOTLOADER PROJECT.
I just want to ask , how TOTAL_FIFO_BYTES has been calculated to (500u + 99u) and why STRUCT_LEN is 20u ??
Hi,
STRUCT_LEN is a length of tFifoInfo which is 20.
It seems the documentation does not corresponds to the latest source files because I can see this in the multi_cyc_fifo.h:
#ifdef EN_LIN_TP
#define TOTAL_FIFO_BYTES (450u) /*config total bytes*/
#elif defined EN_CAN_TP
#define TOTAL_FIFO_BYTES (800u) /*config total bytes*/
#else
#define TOTAL_FIFO_BYTES (100u) /*config total bytes*/
#endif
That should be expected max size considering different TP layers.
Regards,
Lukas
That was copied from this file:
..\S32K1xx_unified_bootloader_demo_V1.0\S32K1xx\UDS_stack\unified_bootloader_stack\Source\FIFO\inc\multi_cyc_fifo.h
from this package:
which was uploaded 2020-03-23.
I believe you have the same version.
Regards,
Lukas