about the function limit of EB Tresos Studio 29.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about the function limit of EB Tresos Studio 29.0

ソリューションへジャンプ
331件の閲覧回数
cranes
Contributor III

Hello,

I am trying to use the AutoSAR example project for S32K344.

When I am configuring the project in EB Tresos and run "im- and exporters", there is only one option in the dropdown list as below screenshot.

cranes_0-1717890750156.png

Does anyone know if this software only provides this option or I miss anything in installing and using the software?

The software is downloaded from here:

cranes_0-1717891163176.png

Thanks!

Crane

 

0 件の賞賛
返信
1 解決策
291件の閲覧回数
cranes
Contributor III

Got it. Thanks Julian!

Regards,

Crane

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
299件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @cranes,

Unfortunately, this is a licensing limitation issue. I recommend contacting EB Tresos to get full version of im- and exporters.

Best regards,
Julián

0 件の賞賛
返信
295件の閲覧回数
cranes
Contributor III

Hi,

So, it means the license from the activation code provided in the SDK doesn't support full version of im- &exporters, right? 

Thanks!

Crane

293件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @cranes,

Yes, that is correct.

0 件の賞賛
返信
292件の閲覧回数
cranes
Contributor III

Got it. Thanks Julian!

Regards,

Crane

0 件の賞賛
返信