about AMMCLIB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about AMMCLIB

1,527件の閲覧回数
letseatorange
Contributor III

I use S32DS with pe, how can i use the AMMCLIB

thanks

0 件の賞賛
返信
1 返信

1,005件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

if you want to use AMMCLIB for S32K microcontroller with S32 Design Studio for ARM version 1.3, please find S32DS installation folder and there is S32K14x_AMMCLIB_v1.1.6 folder which contains all necessary information (including all files and documentation).

Then create new project in S32DS and choose AMMCLIB in startup wizard (please see figure below).

pastedImage_2.png

If you want to use AMMCLIB for KEA microcontrollers, there is the same procedure as I wrote above, but this library is placed in KEAx_AMMCLIB_v1.1.6 folder.

Best Regards,

Martin

0 件の賞賛
返信