What is the output voltage level of FLEXCAN in S32k142?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the output voltage level of FLEXCAN in S32k142?

1,482件の閲覧回数
nishin_jude
Contributor II

Hi,

May I know what is the output voltage level of FLEXCAN in S32K142. Is it 3.3V or 5V?

Thanks and Regards,

Nishin Jude C Abraham

3 返答(返信)

1,331件の閲覧回数
nishin_jude
Contributor II

The FLEXCAN is interoperable with 3.3V and 5V CAN bus. Hence the issue is solved

0 件の賞賛
返信

1,331件の閲覧回数
nishin_jude
Contributor II

Hi Jorge Antonio ,

Thank you for the quick reply. The FLEXCAN transceiver being used on S32K142 is UJA1169TK/F. The datasheet of this transceiver tells that its supply voltage is 5V. So even if, I am changing the supply voltage of the MCU to 3.3 V, will this be able to change the output level for the FLEXCAN to 3.3V ?

0 件の賞賛
返信

1,331件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Nishin Abraham Chakkalakkal

Depends on the power supply of VDD, please check following post:

S32k144EVB Pinout 3.3V not 5V 

Hope it helps

Best regards