Using the DDR tool of S32DS 3.5 to verify that there is a problem with DDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the DDR tool of S32DS 3.5 to verify that there is a problem with DDR

315件の閲覧回数
WX_H
Contributor I

Hello, I timed out when I used the DDR tool of S32 DS3.5 to generate the DDR parameter. The DDR tool can recognize the serial port and make sure that the string number is correct.The crystal frequency is also 40m.The S32E chip is also running normally, but it is not known that the connection timed out, as shown in the following figure.I look forward to your reply.
Best wishes.

スポイラ
S32E DDR企业微信截图_16848234188230.png

 

タグ(2)
0 件の賞賛
返信
0 返答(返信)