Hello, I timed out when I used the DDR tool of S32 DS3.5 to generate the DDR parameter. The DDR tool can recognize the serial port and make sure that the string number is correct.The crystal frequency is also 40m.The S32E chip is also running normally, but it is not known that the connection timed out, as shown in the following figure.I look forward to your reply.
Best wishes.