Using FRDM33771CSPEVB and S32K142EVB-Q100 to build a BMS system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using FRDM33771CSPEVB and S32K142EVB-Q100 to build a BMS system

Jump to solution
1,927 Views
Zyuan17
Contributor III

Hi, I am current try to use these two boards to build a BMS system, including monitoring output voltage and current, implementing algorisms to estimate the battery SOC and SOH, battery balance system and build a GUI.

I encounter some problems and I want to ask these questions:

1. Is there any difference between S32K144EVB-Q100 and S32K142EVB-Q100, I have checked the datasheet of both boards, and there is no difference between the features of these two boards. (Only the chip)
2. Can I download the SREC for the S32K142EVB-Q100 through MC33771C/772C Evaluation GUI
3. Is there any sample codes for the FRDM33771CSPEVB?

Best

0 Kudos
Reply
1 Solution
1,842 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, based on the information I got, it looks like the GUI is written only for S32K144EVB, so S32K142 is not an option.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
7 Replies
1,902 Views
Zyuan17
Contributor III

I am currently using S32K142EVB-Q100, and it is connected to com3, but there are no S32K142 drive shows in the pop-up window. And when I click the PackCtrl, the GUI shows that the EVB is not connected.

Zyuan17_0-1664544349124.png

Zyuan17_1-1664544723146.png

 

Best,
Zhe

 

0 Kudos
Reply
1,908 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,
1. The features are the same, the signals are the same on pin headers but the design is slightly different. You can check the schematics of both boards, you will see some small differences there.

2. See "Initial Configuration" in c:\Program Files (x86)\NXP\MC3377xC EvalGUI\help.chm

lukaszadrapa_0-1664544043041.png

 

3. Take a look at this page:
https://www.nxp.com/design/analog-expert-software-and-tools/sdk-analog-expert-drivers/embedded-sw-ba...

Direct link:
https://www.nxp.com/webapp/Download?colCode=EMBEDDED-SW-BCC-MC33771C&appType=license

Regards,
Lukas

0 Kudos
Reply
1,900 Views
Zyuan17
Contributor III
And could I use the Arduino Uno to control the FRDM33771CSPEVB? Is it an easier solution?
0 Kudos
Reply
1,881 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, you can use any microcontroller with 2 SPI modules. It's just about your requirements.

Regards,

Lukas

0 Kudos
Reply
1,860 Views
Zyuan17
Contributor III

I am currently using S32K142EVB-Q100, and it is connected to com3, but there are no S32K142 drive shows in the pop-up window. And when I click the PackCtrl, the GUI shows that the EVB is not connected.

0 Kudos
Reply
1,843 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, based on the information I got, it looks like the GUI is written only for S32K144EVB, so S32K142 is not an option.

Regards,

Lukas

0 Kudos
Reply
1,854 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Let me ask around if the GUI accepts also S32K142. I'm not really sure. I will let you know later.

Regards,

Lukas

0 Kudos
Reply