Using FRDM33771CSPEVB and S32K142EVB-Q100 to build a BMS system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using FRDM33771CSPEVB and S32K142EVB-Q100 to build a BMS system

ソリューションへジャンプ
1,240件の閲覧回数
Zyuan17
Contributor III

Hi, I am current try to use these two boards to build a BMS system, including monitoring output voltage and current, implementing algorisms to estimate the battery SOC and SOH, battery balance system and build a GUI.

I encounter some problems and I want to ask these questions:

1. Is there any difference between S32K144EVB-Q100 and S32K142EVB-Q100, I have checked the datasheet of both boards, and there is no difference between the features of these two boards. (Only the chip)
2. Can I download the SREC for the S32K142EVB-Q100 through MC33771C/772C Evaluation GUI
3. Is there any sample codes for the FRDM33771CSPEVB?

Best

0 件の賞賛
1 解決策
1,155件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, based on the information I got, it looks like the GUI is written only for S32K144EVB, so S32K142 is not an option.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
7 返答(返信)
1,215件の閲覧回数
Zyuan17
Contributor III

I am currently using S32K142EVB-Q100, and it is connected to com3, but there are no S32K142 drive shows in the pop-up window. And when I click the PackCtrl, the GUI shows that the EVB is not connected.

Zyuan17_0-1664544349124.png

Zyuan17_1-1664544723146.png

 

Best,
Zhe

 

0 件の賞賛
1,221件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,
1. The features are the same, the signals are the same on pin headers but the design is slightly different. You can check the schematics of both boards, you will see some small differences there.

2. See "Initial Configuration" in c:\Program Files (x86)\NXP\MC3377xC EvalGUI\help.chm

lukaszadrapa_0-1664544043041.png

 

3. Take a look at this page:
https://www.nxp.com/design/analog-expert-software-and-tools/sdk-analog-expert-drivers/embedded-sw-ba...

Direct link:
https://www.nxp.com/webapp/Download?colCode=EMBEDDED-SW-BCC-MC33771C&appType=license

Regards,
Lukas

0 件の賞賛
1,213件の閲覧回数
Zyuan17
Contributor III
And could I use the Arduino Uno to control the FRDM33771CSPEVB? Is it an easier solution?
0 件の賞賛
1,194件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, you can use any microcontroller with 2 SPI modules. It's just about your requirements.

Regards,

Lukas

0 件の賞賛
1,173件の閲覧回数
Zyuan17
Contributor III

I am currently using S32K142EVB-Q100, and it is connected to com3, but there are no S32K142 drive shows in the pop-up window. And when I click the PackCtrl, the GUI shows that the EVB is not connected.

0 件の賞賛
1,156件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, based on the information I got, it looks like the GUI is written only for S32K144EVB, so S32K142 is not an option.

Regards,

Lukas

0 件の賞賛
1,167件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Let me ask around if the GUI accepts also S32K142. I'm not really sure. I will let you know later.

Regards,

Lukas

0 件の賞賛