Unable to establish connection to the board S32K148EVB-Q176 using FreeMaster Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to establish connection to the board S32K148EVB-Q176 using FreeMaster Tool

474 Views
Chirag_Dhingra
NXP Employee
NXP Employee

The port is showing on the Freemaster tool but unable to detect the board S32K148EVB-Q176 , please refer to screenshots for error code.

Tags (2)
0 Kudos
1 Reply

468 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Chirag_Dhingra,

Once the OpenSDA if power through USB cable, the port will showing on the FreeMASTER tool. But have you add FreeMASTER codes in your project?

You can test the freemaster_s32k148 example in S321xx SDK RTM v4.0.2 or create your own project by refer to FreeMASTER How To

J8 connect pin 2-3, select P5V_SDA_PSW(USB OpenSDA) to power the MCU.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos