Tracealyzer for S32K344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tracealyzer for S32K344

188 Views
dixonsco
Contributor III

We want to use Percepio Tracealyzer with FreeRTOS on the S32K3 but Tracealyzer's built-in support does not include NXP RTD. I'm hoping someone can either point to an example port of trcHardwarePort.h using RTD or if there is a CMSIS release for the S32K344?

Thanks.

0 Kudos
1 Reply

167 Views
nehalp
Contributor III


Are you looking to stream over UDP/TCP/ or something else?

I'm successfully using Tracealyzer with SafeRTOS (which shares some lineage FreeRTOS) via JLINK RTT on S32K344 with no NXP RTD dependencies.

0 Kudos