I want to use 344MCU to capture a way of PWM duty cycle, it seems that only with interrupts + SAIC mode to achieve duty cycle capture, but I can not use interrupts. I figured out if I could configure two pins, one pin to capture the pulse width (IPWM mode) , the other pin to capture the pulse frequency (IPM mode) , then connect the two pins together and then connect the PWM waveform to be captured, ah, with the pulse width and pulse frequency to get the duty cycle.
What I don't understand is that if I connect the two pins of the MCU together, will the two pins interfere with each other while capturing the PWM signal?
已解决! 转到解答。
2.Emios_Mcl_Ip:
3.Emios_Icu:
4.demo init ipwm and ipm:
5.demo get duty:
Hi
Have you already referred to S32K344_Example_Emios_Icu_IPWM_measurement_DS34_RTD_100_v2?
If you want to use polling method instead of interrupt method, please poll the status via Emios_Icu_Ip_GetInputState before calling Emios_Icu_Ip_GetDutyCycleValues.
Since I don't know the S32K3 RTD version you are using, I sent you the S32K344_Example_Emios_Icu_IPWM_measurement_S32DS35_RTD400.zip through private message. It is recommended to modify it to the polling mode based on project. Sorry, I haven't had time to test the polling method for you because I have been dealing with a lot of cases recently. If you still can't implement it after the modification, please let me know.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Sorry, I just noticed the message now. Here is the program provided by technical support, but it should still be the interrupt capture PWM duty cycle method. The actual implementation using polling can be seen in my solution below, which has been verified.
2.Emios_Mcl_Ip:
3.Emios_Icu:
4.demo init ipwm and ipm:
5.demo get duty: