Error in services launch sequence
PEmicro GDB Launch Failure : The GDB Server was not able to establish a connection to the target processor. Please check your connections and power. Verify that the launch settings in the Debug Configuration are accurate.
i use my own pcb,
S32 Design Studio for ARM Version: 2018.R1 Build id: 180815
chip:S32K116.
Or there is one more possibility that your watchdog is not disabled.
Best Regards,
Ajay Yadav
Hello Xinyu and Robin,
I was facing same issue and going through comments on software forum, As I am looking into older comments on forum in future someone like me may reach this thread and he might get benefitted from my comment so adding it to this thread.
I found that issue was present with my PE micro hardware (It was faulty), I was able to find root cause with Kinetis Recovery utility tool.
To download it, Follow below link,
Solved: Can't use PEmicro debugger with S32K118EVB2-Q048 - NXP Community
Best Regards,
Ajay Yadav
Hi xinyu1650,
Have you check the connections and power?
Have you successfully program the chip before?
Please observe the waveform of the RESET pin with an oscilloscope and upload a picture. If there is a periodic pulse, please let me know the period of the pulse.
Have you tried to using P&E Recovery Utility halt MCU by refer to: https://community.nxp.com/t5/S32K/Can-t-use-PEmicro-debugger-with-S32K118EVB2-Q048/td-p/1376204
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
No change in pin voltage(reset and vcc pin),the voltage is 0v.
Would you please power the S32K116?