TJA1128- Temperature profile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1128- Temperature profile

Jump to solution
726 Views
Kavin_Kumaravel
Contributor II

what is the maximum temperature TJA1128 could withstand and for how long continuously? or what is the duration of maximum temperature it could withstand over the life time?

STRESS TEST: I am having an issue, that temperature of TJA is maintained at 130 deg for 600 seconds in every 8400 second cycle and repeat the same cycle for 150 cycles. and It failed to communicate after that and regained communication once temperature is (after some time) lowered and reset.

 

Any ideas?

0 Kudos
Reply
1 Solution
704 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Kavin,

I hope all is great with you. Thank you for using the NXP communities.

Please review the response from our specialist below:

It really comes down to the operational or storage temperature.

For storage temperature, the max is -55°C to 150°C without time limit.

For the operational temperature, the device virtual junction temperature shall not exceed 150°C (keep in mind the junction will be hotter than ambient).

Any excursion above this may damage the device.

The datasheet parameters are guaranteed to the same temperatures except where noted in the datasheet.

 

Regarding your testing, the device does have overtemp shutdown protection.

diazmarin09_0-1684516084920.png

I hope this information helps.

Regards,

David

View solution in original post

0 Kudos
Reply
4 Replies
658 Views
Kavin_Kumaravel
Contributor II
How do I can calculate Power dissipation of TJA1128?
0 Kudos
Reply
645 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Kavin,

I am pleased to contact you again.

In that case, I do recommend reviewing the following document from your secure files:

diazmarin09_0-1684877177644.png

 

I hope this information helps.

Regards,

0 Kudos
Reply
681 Views
Kavin_Kumaravel
Contributor II

Thank you David, I am sure I found the root cause.

0 Kudos
Reply
705 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Kavin,

I hope all is great with you. Thank you for using the NXP communities.

Please review the response from our specialist below:

It really comes down to the operational or storage temperature.

For storage temperature, the max is -55°C to 150°C without time limit.

For the operational temperature, the device virtual junction temperature shall not exceed 150°C (keep in mind the junction will be hotter than ambient).

Any excursion above this may damage the device.

The datasheet parameters are guaranteed to the same temperatures except where noted in the datasheet.

 

Regarding your testing, the device does have overtemp shutdown protection.

diazmarin09_0-1684516084920.png

I hope this information helps.

Regards,

David

0 Kudos
Reply