Some ADC channel reading 0 in S32K146

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some ADC channel reading 0 in S32K146

739 Views
deepthi_keshava
Contributor I

Inputs considered are on SE0, SE1 and SE5 on ADC0. Back to back triggering has been enabled. If SE5 is disabled, correct values are obtained on the SE0 and SE1 channels. When SE5 input is enabled, all the values (var1, var & var3) show up as 0.

Any help?

PDB0->MOD = 1200;
PDB0->IDLY =1200;

PDB0->CH[0].C1 = (PDB_C1_BB(0x02)
| PDB_C1_TOS(0x01)
| PDB_C1_EN(0x03));

ADC_DRV_ConfigChan(INST_ADCONV1, ADC_INPUTCHAN_EXT0, &adConv1_ChnConfig0);
ADC_DRV_ConfigChan(INST_ADCONV1, ADC_INPUTCHAN_EXT1, &adConv1_ChnConfig1);

ADC_DRV_ConfigChan(INST_ADCONV1, ADC_INPUTCHAN_EXT5, &adConv1_ChnConfig2);

ADC0->SC1[0] = ADC_SC1_ADCH(0); // SC1A[ADCH]
ADC0->SC1[1] = ADC_SC1_ADCH(1); // SC1B[ADCH]
ADC0->SC1[2] = ADC_SC1_ADCH(5); // SC1F[ADCH]

var1 = ADC0->R[0]; 
var2 = ADC0->R[1];
var3 = ADC0->R[5];

0 Kudos
Reply
1 Reply

662 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the setting does not look right for 3 channels conversion in back-to-back mode. You should have 

PDB0->CH[0].C1 = (PDB_C1_BB(0x06) | PDB_C1_TOS(0x01) | PDB_C1_EN(0x07)); 

Channel delay 0 register should be configured too, or simply clear TOS if delay of first sample is not needed.

Also you should read result from R0, R1, R2 registers

var3 = ADC0->R[2];

BR, Petr

0 Kudos
Reply