Hi,
yes, you can.
Strict sequential boot mode is special one as it keeps the device in reset forever when the verification fails.
Failing sequential and parallel boot modes don't do that, you are just not able to use boot protected keys in case of verification fail. But the device is still working without other limitations.
To reset the device back to factory state, you need to know MASTER ECU KEY.
More details and SW example can be found in AN5401:
https://www.nxp.com/webapp/Download?colCode=AN5401&location=null
https://www.nxp.com/webapp/Download?colCode=AN5401SW&location=null
Regards,
Lukas
If the sequential or parallel boot mode fail, BOK bit in FCSESTAT register is cleared and you can't use boot protected keys.
See "3.1.3 Key Attributes" in AN5401 for details.
See also SW examples in the application note. When loading a key, attributes can be added when calling calculate_M1_to_M5() function. It's the last parameter.
Regards,
Lukas
Hi Lukas,
I enabled security boot mode is "Sequential Boot Mode",
but security boot verification failed, could you please determine what went wrong?
The FCSESTAT register value is :
FCSESTAT[SB]=1
FCSESTAT[BIN]=0
FCSESTAT[BFN]=1
FCSESTAT[BOK]=0
Hi,
this means that BOOT_MAC calculated by CSE after reset does not correspond to value stored in BOOT_MAC slot.
Did you followed all the steps described in AN5401?
If you updated the content of flash, BOOT_MAC needs to be updated too. Or you can perform reset to factory state (also described in AN5401) and start over.
Regards,
Lukas
Hi,
no, it's not necessary. But it should be done as it locks CMD_BOOT_FAILURE command. Take a look at:
https://community.nxp.com/t5/S32K/s32k144-csec-Boot-Ok-Command/m-p/1330132
Regards,
Lukas
Hi Lukas,
Now, secure boot verfication is success,i update ted secure boot area code and update BOOT MAC success,but after reset,secure boot failed,What do we need to pay attention to update BOOT MAC