S32k146 Process expert- No active project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k146 Process expert- No active project

ソリューションへジャンプ
765件の閲覧回数
PU1
Contributor II

The  pop up window comes, when I try to generate code . 

I'm am using DS32 ARM 2.2 

pop when try to generate codepop when try to generate code

Also not able to add module to projectwhen try to add module no option is not enablewhen try to add module no option is not enable

0 件の賞賛
返信
1 解決策
626件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that your project is baremetal without SDK included. Please refer to the Attaching an SDK to an existing project of S32DS_ARM_User_Guide.pdf.

Attaching an SDK to an existing project.png

Please select the SDKs next time you create a new project.

Select SDK.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
608件の閲覧回数
PU1
Contributor II

Thanks for your reply  @Robin_Shen,

i was following same procedure.

my issue is solved. ,,some packages are not added.

0 件の賞賛
返信
627件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that your project is baremetal without SDK included. Please refer to the Attaching an SDK to an existing project of S32DS_ARM_User_Guide.pdf.

Attaching an SDK to an existing project.png

Please select the SDKs next time you create a new project.

Select SDK.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------