S32KDS bulid S32K312 project very slow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32KDS bulid S32K312 project very slow

579件の閲覧回数
Ean
Contributor II

project is a UART example.20240508-145609222.jpg

 20240508-145355.jpg

タグ(1)
0 件の賞賛
返信
5 返答(返信)

549件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ean,

Firstly, please make sure your device meets the minimum requirements for S32DS:

Julin_AragnM_0-1715203703199.png

If build time is still slow when meeting the requirements, you can increase RAM usage from s32ds.ini file (located in C:\NXP\S32DS.3.5\eclipse\folder). The variable "Xmx" is the maximum RAM that can be used by S32DS, you could increase the value, depending on your machine.

Best regards,
Julián

0 件の賞賛
返信

516件の閲覧回数
Ean
Contributor II
i disconnect computer wifi.can fix this problem,but why?
0 件の賞賛
返信

476件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ean,

Could you share which version of Design Studio you are using? There have been some reports on old tools for slow build time that has been fixed by disconnecting the network, such as these:

Best regards,
Julián

0 件の賞賛
返信

473件の閲覧回数
Ean
Contributor II

1.jpg2.jpg3.jpg

0 件の賞賛
返信

439件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ean,

S32DS should not have any dependency on network, could it be some background process slowing down compilation time?

Perhaps you could try to capture network traffic until the build process is finished (e.g. via a network sniffer like Wireshark)?  Then you might also try to identify which process owns the TCP connection suspected of the build delays (e.g. TCPView).

You could also try updating to newest RTD release to test compilation times.

Best regards,
Julián

0 件の賞賛
返信