S32K3xx: S32DS Platform IDE: Change controller for an existing S32DS project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3xx: S32DS Platform IDE: Change controller for an existing S32DS project

Jump to solution
405 Views
tecprasant
Contributor II

Hi,

I have used S32DS Platform IDE and created a project for S32K3x4 IC. I would now like to change this project to S32K31x controller.

What is the best way to update an existing project? 
Is there any document highlighting the steps required to make this change?

 

I want to avoid creating a fresh project from scratch.

 

Any inputs will be of help.

 

Regards

0 Kudos
Reply
1 Solution
380 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @tecprasant,

Currently, the most viable option is to generate a new project with the desired part number and copy your application source files from the pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience.

Best regards,
Julián

View solution in original post

0 Kudos
Reply
4 Replies
311 Views
tecprasant
Contributor II

Thanks @Julián_AragónM . This information makes it very clear for me.

381 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @tecprasant,

Currently, the most viable option is to generate a new project with the desired part number and copy your application source files from the pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience.

Best regards,
Julián

0 Kudos
Reply
323 Views
tecprasant
Contributor II

@Julián_AragónM : Thanks for the inputs. This answers my query.

I have an additional query: If I want to only change the MCU package, say from S32K344 172 pin package to 100 pin package, then what is recommended?
(a) I create a new project?
(b) I change the package in the NXP package selection (in the same project) ?

 

Regards,

0 Kudos
Reply
317 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @tecprasant,

For changing the package, this can be done inside the S32DS Config Tool (option b), just keep in mind the difference between these packages and modify the pin configurations accordingly.

Julin_AragnM_0-1715702816302.png

Best regards,
Julián

0 Kudos
Reply