Dear
About LWIP Network stack
When loading the lwip stack, an assertion occurs in rand() as shown in the log below.
assertion "REENT malloc succeeded" failed: file "../../../../../../../../src_newlib/newlib/libc/stdlib/rand.c", line 78
It operates normally if the related rand() is removed or newlib is set to no I/O like picture
We are in an environment that uses FreeRTOS + LWIP + MbedTLS(HSE),
Please guide me on which newlib to use and how to correct the above problem to accurately resolve it.
Additional reproduction comment.
A1. make sample project for RTD testing.
A2. change as newlib semihost or newlib nano semihost in library support
A3. add rand() in main function.
A4. run and test
or
B1. make FreeRTOS + LWIP + MbedTLS(HSE) project
B2. do as A2 , A3, A4
compare Between A & B, check if working is ok?