Hello,
Based on the minimum system board (all IOs are floating) of S32K34x, the low power mode result is as Datasheet.
Hope will be helpful for you as reference.
Cheers !
Oliver
已解决! 转到解答。
S32K3 mini EVB:
* Support both S32K344 and S32K312 (HDQFP172);
* All GPIO extended out;
* 1 User LED (can be routed to any pin), 1 reset LED, 1 power LED;
* 1 User switch (can be routed to any pin), 1 reset switch;
* Can be programmed by 10 pin JTAG debug port or 5pin SWD debug header;
* Power the MCU by type C(5V) cable or Header H1 (VDD_HV_A and B have to be the same voltage);
* I2C pull up resisters(Can be routed to any I2C pin);
* 16MHZ crystal;
* Size: 9x7cm;
S32K3 mini EVB:
* Support both S32K344 and S32K312 (HDQFP172);
* All GPIO extended out;
* 1 User LED (can be routed to any pin), 1 reset LED, 1 power LED;
* 1 User switch (can be routed to any pin), 1 reset switch;
* Can be programmed by 10 pin JTAG debug port or 5pin SWD debug header;
* Power the MCU by type C(5V) cable or Header H1 (VDD_HV_A and B have to be the same voltage);
* I2C pull up resisters(Can be routed to any I2C pin);
* 16MHZ crystal;
* Size: 9x7cm;