I made a program with flexcan sdk and I debug on the EVB.
The program can send can message but not all the time .
For example the first time download elf file and run can send the can message successful but the second time download elf file and run cannot send the can message.
Why this happened? Please help me solve this problem.
And the attach file is the program.
解決済! 解決策の投稿を見る。
Hi,
could below thread be useful for you?
https://community.nxp.com/t5/S32K/S32K344-Evaluation-Board-FlexCan-Example-running/m-p/1343355
If using S32K3X4EVB-Q257, there is secure CAN transceiver on the board, TJA1153, which is not configured by default and it does not allow the MCU to communicate with the CAN bus. So a config must be done first.
BR, Petr
Hi,
could below thread be useful for you?
https://community.nxp.com/t5/S32K/S32K344-Evaluation-Board-FlexCan-Example-running/m-p/1343355
If using S32K3X4EVB-Q257, there is secure CAN transceiver on the board, TJA1153, which is not configured by default and it does not allow the MCU to communicate with the CAN bus. So a config must be done first.
BR, Petr
Thank you the problem is solved