Hi, I have the S32K344-WB Evaluation Board. I am following this guide. I have installed all the packages listed on the "Get Software" page.
I am importing an example project as shown here: https://www.nxp.com/webapp/Download?colCode=UG10049
I've imported the "s32k3_wb_self_test" project. I get the error "Mcal.h: No such file or directory" when trying to build the project.
I'm guessing it is because I'm missing these libraries?
Please help. Thanks.
Solved! Go to Solution.
Ah, that was the issue. I was using the latest version of the IDE, 3.5, instead of the version the guide called out to use, 3.4. This in turn led me to use newer versions of the SDK, which I think was the issue. It builds now.
Here is my test, i see no prblem on myside.
So please double check the IDE and RTD version you're using.
Ah, that was the issue. I was using the latest version of the IDE, 3.5, instead of the version the guide called out to use, 3.4. This in turn led me to use newer versions of the SDK, which I think was the issue. It builds now.